Error Management
When a non-fatal error occurs and motion must be stopped quickly, the following procedure can be taken:
For each axis:
|
Step |
Example Application Code |
|---|---|
|
Send Stop Command for each axis |
MLAxisStop(PipeNetwork.AXI_A1_Axis, TRUE, DEF_A1_StopDec); |
|
Stop the Axis Motion Generator |
MLAxisMoveVel(PipeNetwork.AXI_A1_Axis, 0.0); |
|
Wait for Axis to be stopped |
AxisStatus := MLAxisStatus(PipeNetwork.AXI_A1_Axis); |
|
Turn power off(disable) all the axes |
MLAxisPower(PipeNetwork.AXI_A1_Axis,FALSE); |
|
Disconnect Pipe Network from the axis |
MLCNVDisconnect(PipeNetwork.CNV_A1); |
For the machine:
|
Step |
Example Application Code |
|---|---|
|
Stop Command at the master block level |
MLMstRun(PipeNetwork.MASTER, 0.0); |
|
Wait for Master command to be stopped |
IF A1_AckState = DEF_StateErrorStop |
This procedure for error management is based on the Project Structure Guidelines as described in Application Software Structure - Implementation
For information on restarting the motion, refer to Restarting Motion with PipeNetwork
|
Copyright © 2018 Kollmorgen |
|